MasterAid 220: Error message when creating file even though there is enough space
Problem:Solution
A description of this resolution:
"MasterAid 220: Error message when creating file even though there is enough space" resolves the following:
A description of this resolution:
- This error will be corrected in the next release of QMA221.
WORKAROUND/SOLUTION
Create a dummy target.
[ref SR3001 VASMASOITA0611 ]
"MasterAid 220: Error message when creating file even though there is enough space" resolves the following:
- MasterAid 220: Error message when creating file even though there is enough space
The creation of a file (PCMASS, etc) within Command Oriented Function may fail stating not enough space left on harddisk. This may occur also if there is enough space left.
This error occurs only if the harddisk has more than about 100 MByte free space.
PRODUCTS CONCERNED
MasterAid 220-FP*1.0/0 - FP*1.2/1
SOFTWARE CONCERNED
Software component:
MasterAid 220 Software (QMA221)
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment