MasterAid 220: Problem with DUTPT
Problem:Solution
A description of this resolution:
"MasterAid 220: Problem with DUTPT" resolves the following:
A description of this resolution:
- This error will be corrected in the next revision of the products concerned.
There is no possibility to circumvent the problem with the DUTPT command.
[ref SR2093 VASMASOITA0613 ]
"MasterAid 220: Problem with DUTPT" resolves the following:
- MasterAid 220: Problem with DUTPT
There is an error in the dump segment handling of the DUTPT command within the MasterAid 220 software.
The error occurs if the dump size is 1MB, 2MB, 3MB... or very close to that size. DUTPT calculates that a an additional segment is neccessary to keep the dump information, but the segment is never created. The dump can’t be loaded with the LOTDB command.
PRODUCTS CONCERNED
MasterAid 220-FP*1.2/1:
MasterAid 220 Upgrade Software; 3.5" and 5.25"
Command Oriented Functions (QMA221)
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment