MasterAid 220: Convert MA 220 -> MA 215, User diskette
Problem:Solution
A description of this resolution:
'MasterAid 220: Convert MA 220 -> MA 215, User diskette' resolves the following:
A description of this resolution:
- The error will be corrected in the next revision 1.2/1.
To circumvent this problem use the RENAME function on MasterAid 215. Start a local session on MasterAid 215 and use the command:
RENAME USER:*.*>*.*;RW
do not mind the message DIR$USER.MM is busy.
[ref SR2047 VASMASOITA0614 ]
'MasterAid 220: Convert MA 220 -> MA 215, User diskette' resolves the following:
- MasterAid 220: Convert MA 220 -> MA 215, User diskette
When converting the MasterAid 220 User directory to a MasterAid 215 USER diskette, all files on this USER disk will be set to read only. This will cause a fatal error on MasterAid 215 during startup of a session when using this diskette.
Error Message : ... 21 15 DECC200 ... 136 ... 19 10 DECC200 A ... press
PRODUCTS CONCERNED
MasterAid 220-FP*1.2/0:
MasterAid 220 Upgrade Software; 3.5' and 5.25'
MasterAid 220 Software for MP 90; 3.5' and 5.25'
SOFTWARE CONCERNED
Software component:
MasterAid 220 Software (QMA220)
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment