MasterAid 220: Convert MA 220 -> MA 215. Input: DUTDB dump on SRCE:
Problem:MasterAid 220: Convert MA 220 -> MA 215. Input: DUTDB dump on SRCE:Solution
A description of this resolution:
"MasterAid 220: Convert MA 220 -> MA 215. Input: DUTDB dump on SRCE:" resolves the following:
A description of this resolution:
- The error will be corrected in the next revision 1.2/1.
To circumvent this problem:
Use a MasterAid 215 to initiate some empty diskettes with the name DUD1 ... DUD*:
e.g. INIT DUD1,0,63
Afterwards use a MasterAid 215 to copy all files from the diskettes "DUP*" to "DUD*":
e.g. COPY DUP1:*.*>DUD1*.*
With these new diskettes you can start the command LOTDB as usual.
[ref SR2046 VASMASOITA0615 ]
"MasterAid 220: Convert MA 220 -> MA 215. Input: DUTDB dump on SRCE:" resolves the following:
- MasterAid 220: Convert MA 220 -> MA 215. Input: DUTDB dump on SRCE:
When converting a DUTDB dump prepared on MasterAid 220 to MasterAid 215 diskettes, this will get wrong volume names (DUP* instead of DUD*). This will cause an error when you try to load the dump on MasterAid 215 because the command LOTDB expects diskettes with volume names like DUD*. In this situation you should terminate the load command in the following way:
#LOTDB
#Enter name of Base volume (
INSERT VOLUME DUD1 ! READY (Y/N/Q) = Q
If you enter the volume name of the inserted diskette, you should terminate the command in the following way:
#LOTDB
#Enter name of Base volume (
-- -- error! -- -- invalid base volume name!
Base volume name is DUD1 ! Continue (Y/N/Q) = Y
INSERT VOLUME DUD1 ! READY (Y/N/Q) = Q
PRODUCTS CONCERNED
MasterAid 220-FP*1.2/0:
MasterAid 220 Upgrade Software; 3.5" and 5.25"
MasterAid 220 Software for MP 90; 3.5" and 5.25"
SOFTWARE CONCERNED
Software component:
MasterAid 220 Software (QMA220)
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment