MasterPiece 90 - System Software loading
Problem:Solution
A description of this resolution:
'MasterPiece 90 - System Software loading' resolves the following:
A description of this resolution:
- This behaviour will be corrected with the next revision of MasterPiece 90.
Workaround: When the described conditions are met, enter the following commands from the MS-DOS command line:
(note the name of the *.IMG file)
LOADER -N name.IMG
This procedure assumes that the disk containing the QMPxx option or QMPxx to QMPyy upgrade is in drive A: of the computer.
Change ’A:’ to ’B:’ if the the disk is in drive B:
[ref SR3007 VASMASOITA0681 ]
'MasterPiece 90 - System Software loading' resolves the following:
- MasterPiece 90 - System Software loading
With fast MasterAid computers equipped with a 486 CPU, it might happen that the MasterPiece 90 Loader terminates with the error message 'MP90 doesn’t respond' while the PM630 still shows ’PL’ in its seven segment display.
PRODUCTS CONCERNED
MasterPiece 90
SOFTWARE CONCERNED
Options: QMP92 1.2
QMP93 1.2
QMP94 1.2
QMP95 1.2
Upgrades: QMP92 1.2 TO QMP93 1.2
QMP92 1.2 TO QMP94 1.2
QMP93 1.2 TO QMP95 1.2
QMP94 1.2 TO QMP95 1.2
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment