MasterBatch 200 - Periodical savings of configuration files
Problem:Solution
A description of this resolution:
"MasterBatch 200 - Periodical savings of configuration files" resolves the following:
A description of this resolution:
- The error will be corrected in the next revisions of MasterBatch 200/1*5.0 and MasterBatch 200/1*5.1.
Workaround:
Set a period of 24 hours or less.
[ref FKP1048 VASMASOITA0649 ]
"MasterBatch 200 - Periodical savings of configuration files" resolves the following:
- MasterBatch 200 - Periodical savings of configuration files
If an interval time of more than 30 hours is specified overflow will occur. This makes the interval time negative and when the system calculates the next saving time, an earlier time is obtained and the file is saved immediately.
PRODUCT CONCERNED
MasterBatch 200/1.
SOFTWARE CONCERNED
MBC200/1*5.0/0
MBC200/1*5.1/0
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment