Documentation error - MasterPiece 100, Error in PC-element manual for KEYB-GR
Problem:Solution
A description of this resolution:
"Documentation error - MasterPiece 100, Error in PC-element manual for KEYB-GR" resolves the following:
A description of this resolution:
- CORRECTION
In the last paragraph under the headline GROUP FUNCTION, SEVERAL KEYS
The outputs ACTC is set to 1 as long as a key in the corresponding group is depressed, independent of the value on the corresponding inputs EN and R.
[ref TMP0127 VASMASOITA0664 ]
"Documentation error - MasterPiece 100, Error in PC-element manual for KEYB-GR" resolves the following:
- Documentation error - MasterPiece 100, Error in PC-element manual for KEYB-GR
MANUALS CONCERNED
English:
ABB MasterPiece PC elements 7650 063-208 and older releases
Swedish:
ABB MasterPiece PC-element 7650 063-108 and older releases
PAGES CONCERNED
Page 14:11
PC element KEYB-GR
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment