MasterPiece 90 - PC-elements REG-G and FUNG-1V
Problem:Solution
A description of this resolution:
'MasterPiece 90 - PC-elements REG-G and FUNG-1V' resolves the following:
A description of this resolution:
- This problem will be corrected with the next revision of MasterPiece 90.
Workaround: Do not place the REG-G and FUNG-1V PC-element in different control modules.
[ref SR4002 VASMASOITA0670 ]
'MasterPiece 90 - PC-elements REG-G and FUNG-1V' resolves the following:
- MasterPiece 90 - PC-elements REG-G and FUNG-1V
The transfer of GROUP-data between a REG-G PC-element in one control module and the FUNG-1V PC-element in another control module does not work correctly.
PRODUCTS CONCERNED
MasterPiece 90
SOFTWARE CONCERNED
Options: QMP92 1.2/x
QMP93 1.2/x
QMP94 1.2/x
QMP95 1.2/x
Upgrades: QMP92 1.2/x TO QMP93 1.2/x
QMP92 1.2/x TO QMP94 1.2/x
QMP93 1.2/x TO QMP95 1.2/x
QMP94 1.2/x TO QMP95 1.2/x
where x is = 1,2,3
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment