Flat screen with Advant OS
Problem:Solution
A description of this resolution:
"Flat screen with Advant OS" resolves the following:
A description of this resolution:
- Flat screen with Advant OS
The following flat screens monitors have been used with Advant Station and X-terminals. NEC 18 inch,NEC LCD 2010, and the TFT monitors the 15 and 20 inch.
"Flat screen with Advant OS" resolves the following:
- Flat screen with Advant OS
Flat Screen With Advant OS
must also be able to work with a 15m extention cable
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment