Advant Controller 410/450 and MasterPiece 200/1 - PC element MOTCON must have Operator Station support
Problem:Solution
A description of this resolution:
"Advant Controller 410/450 and MasterPiece 200/1 - PC element MOTCON must have Operator Station support" resolves the following:
A description of this resolution:
- This problem will not be corrected.
[ref SR5050 VASMASOITA0131 ]
"Advant Controller 410/450 and MasterPiece 200/1 - PC element MOTCON must have Operator Station support" resolves the following:
- MOTCON can not be used without the program modules supporting Operator Station
The PC element MOTCON can not be used without the following program modules installed in the system (support for Operator Station):
Advant Controller 410: QC01-OPF11
Advant Controller 450: QC02-OPF21
MasterPiece 200/1: QMV800
If one tries there will be no control action in MOTCON but instead an overflow of system messages 22 10 DAXI002 111 (or 112) .........
Products concerned
Advant Controller 410*1.0/x x = 0,1,2,3
Advant Controller 450*1.0/x
MasterPiece 200/1*4.0/y y = 2,3,4,5,6,7,8
Software concerned
QC01-BAS11*7.0/z z = 0,1,2,3
QC02-BAS21*7.0/z
QMP280 SW*6.0/u u = 2,3,4,5,6
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment