PCV02 with hazeltine on Line A and ConLink on Line B
Problem:Solution
A description of this resolution:
"PCV02 with hazeltine on Line A and ConLink on Line B" resolves the following:
The underlying cause is:
A description of this resolution:
- Handling
Please observe the following handling:
- Avoid the utilization of a PCV02 with hazeltine handler on Line A and ConLink with tag transfer on Line B. If the above cannot be avoided, the entry into the configuration dialog may only take place with stopped tag transfer.
"PCV02 with hazeltine on Line A and ConLink on Line B" resolves the following:
- ConLink
If a PCV02 is configured with hazeltine on Line A and ConLink on Line B, upon entry with the hazeltine in the configuration dialog, the ConLink data transfer (tag trf) is interrupted.
Consequences: Restart of the data transmission after station stop/start.
The underlying cause is:
- Software error
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment