Recipe processing
Problem:Solution
A description of this resolution:
"Recipe processing" resolves the following:
The underlying cause is:
A description of this resolution:
- Reset the operator station
Handling:
Texts of recipe controls may be changed only when operator station is not running.
In case of error:
In case of error an operator station reset (e.g. stop/start) will be required.
"Recipe processing" resolves the following:
- Recipe
If texts are changed in the configuration dialog of the processing recipe control when a control recipe is running the relevant active control recipe in the DISPO will not continue being processed by this recipe control.
Symptoms:
- Recipe sticks and next phase does not start respectively; No END time is entered for the active phase; System error message RECIPE PROCESSING ERROR; Message on alarm page OPEN/FAULTY ACCESS TO RECIPE.
The underlying cause is:
- Handling error
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment