Selection of 4th monitor
Problem:Solution
A description of this resolution:
"Selection of 4th monitor" resolves the following:
The underlying cause is:
A description of this resolution:
- Select RELEASE + M3
SELECTION is done with RELEASE + M3.
For the local operator panel the 3rd and 4th monitor are selected with SHIFT + M1 and SHIFT + M2.
Shift and release function of the local operator panel are always placed on one key.
"Selection of 4th monitor" resolves the following:
- Operating/Monitoring
With regard to POT73/75, index 7, selection of the 4th monitor does not work.
From firmware version V8.0 on, selecting a 4th monitor calls for index 58 or 8 since this contains EPROM 310 02 64 (index F) which is required for selection.
Indices 58 and 8 only differ from each other in their keyboard foil. Index 58 has the conventional foil. Index 8 has a changed keyboard foil; key M3 is marked with M3/M4.
The underlying cause is:
- Hardware incompatibility
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment