Curve acquisition / box allocation
Problem:Solution
A description of this resolution:
"Curve acquisition / box allocation" resolves the following:
The underlying cause is:
A description of this resolution:
- Releasing the boxes
The following can solve the problem:
- Restart the mass memory Re-enter the curve acquisitions by saving Stop and start a single task with curve acquisition
(Start parameter C000) Stop and start one of the first tasks with curve acquisition
(Start parameter E000)
"Curve acquisition / box allocation" resolves the following:
- Mass memory
It has been noticed that all curve acquisitions independent of the task in the COS no longer write to the mass memory.
The underlying cause is:
- Boxes blocked
A readout of the address 5000:8 L 4 (Box allocation) revealed that the curve acquisitions no longer release the boxes.
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment