DI830/831 incorrect power supervision error handling
Problem:Solution
A description of this resolution:
'DI830/831 incorrect power supervision error handling' resolves the following:
A description of this resolution:
- The problem will be corrected in the next Product Revision PR: E
[ref SR1160 VASMASOITA0026 ]
'DI830/831 incorrect power supervision error handling' resolves the following:
- DI830 and DI831 Product Revision: D or earlier
Sensor power supervision 1 and 2 are mixed up. Sensor power supervision 1 will give error on channel 9 to 16 instead of channel 1 to 8 if low sensor power. Sensor power supervision 2 will give error on channel 1 to 8 instead of channel 9 to 16 if low sensor power. This is only a problem if there are different power supplies connected to sensor power supervision 1 and 2.
- Article imported from the previous version of KnowledgeBank
Add new comment