Process Portal A 2.1/1 - Property Translation may cause crashes in OPC DA (Data Access) Clients
Problem:Solution
- The error has been corrected in Process Portal A 2.1/2
[ref 3BSE029867D0011 VASMASOITA0777 ]
- Process Portal A 2.1/1 - Property Translation may cause crashes in OPC DA (Data Access) Clients
Property Translation may cause OPC Clients, for example System Status viewer, to throw an exception. The result is a huge memory leak in the workplace process. The error occurs e.g. when a system status viewer is opened in the preview area and in an overlap.
- Article imported from the previous version of KnowledgeBank
Add new comment