Process Portal A 2.1/1 - OPC Adapter may never complete transaction if multiple items are read or written
Problem:Solution
- The error has been corrected in Process Portal A 2.1/2
[ref 3BSE029867D0011 VASMASOITA0751 ]
- Process Portal A 2.1/1 - OPC Adapter may never complete transaction if multiple items are read or written
If a read/write is made with multiple items, which have different default update rates (configured in the CCA), the OPC Adapter will complete the transaction, i.e. no response to the client is sent - in case the read/write operation is synchronous, the client will hang.
- Article imported from the previous version of KnowledgeBank
Add new comment