Process Portal A 2.1/1 - Read/Write operations may cause unpredictable result in OPC Adapter
Problem:Solution
- The error has been corrected in Process Portal A 2.1/2
[ref 3BSE029867D0011 VASMASOITA0750 ]
- Process Portal A 2.1/1 - Read/Write operations may cause unpredictable result in OPC Adapter
In the OPC Adapter, a race condition can occur in read and write operations that may in worst case crash the Connector Server, or make it spin. In some cases, the race condition may also cause the read or write transaction to never be completed, which in turn may cause clients to hang.
- Article imported from the previous version of KnowledgeBank
Add new comment