Process Portal A 2.1/1 - The combination, Aspect Link and Windows Application aspect, doesn't work
Problem:Solution
- The error has been corrected in Process Portal A 2.1/2
[ref 3BSE029867D0011 VASMASOITA0742 ]
- Process Portal A 2.1/1 - The combination, Aspect Link and Windows Application aspect, doesn't work
When calling a Windows Application aspect from a Process Graphics Aspect Link, the Configuration View is displayed, instead of starting the configured application. Application Bar and Display Bar short-cuts are not affected by this problem.
- Article imported from the previous version of KnowledgeBank
Add new comment