AC 400 Connect 2.1/0 - AC400C Node Status, OPCDA Connector stop for Node no. < 10
Problem:Solution
- The error has been corrected in AC 400 Connect 2.1/1
[ref 3BSE029820D0002 VASMASOITA0714 ]
- AC 400 Connect 2.1/0 - AC400C Node Status, OPCDA Connector stop for Node no. < 10
If nodes with numbers under 10 was disconnected, the Node Status Server treated the node as a Gate on the Plant network. The result was that all nodes on the same network were reported to be down. This caused the OPCDA service provider process to stop.
- Article imported from the previous version of KnowledgeBank
Add new comment