AC 400 Connect 2.1, MB300 Data Base and Long Cycle Times problems
Problem:Solution
- Install Patch: AC400C2.1_MB300_Patch02
This patch also includes patch AC400C2.1_MB300_Patch01
Installation at least needed on all connectivity server nodes for MB300
[ref SR1153 VASMASOITA0005 ]
- 10 sec subscription will be ignored
1. If you have a 1 sec subscription for an object and then even request a 10 sec subscription for the same object, the 10 sec subscription wll be ignored.
2. The OPC DA Master adapter consumes more handles than the MB300 data base can allocate (patch AC400C2.1_MB300_Patch01).
- Article imported from the previous version of KnowledgeBank
Add new comment