Windows English with DigiVis or CBF and Cyrillic characters
Problem:Solution
- Set RUSSIAN as system default locale
In Windows (WinNT or Win2000), set the Russian as system default locale.
- In Control Panel see Regional Settings - General Click the button "Set default …" . In the dialog "Select System Locale" select "Russian".
After this setting, you will be asked to reboot the PC.
- Operation and Observation
The Operating System of the Operator Station is Windows English.
In Digivis, the Cyrillic characters are supported (Language = Russian).
Problem: The error messages cannot be displayed correctly. The characters in the message list are not readable.
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment