No connection to the Gateway-CPU - CN 37-061 EN
Problem:Solution
- Handling
Check the Gateway-CPU configuration for the correct IP address via DiagnosticInterface, delete the Operating System of the Gateway-CPU and try to connect again.
To delete the Operating System, please contact the ABB Automation Service Support(Phone: + 49 1805 123 580 or e-mail: callcenter.automation@de.abb.com).
- General System Information
DigiTool gets no connection to the Gateway-CPU (e .g. the CPU has a wrong IP address, a wrong Operating System or was booted with another ressource than configured in DigiTool).
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment