The message APPLICATION LOG FILE IS FULL appears when DigiTool is started
Problem:Solution
- Reconfigure the application log in Windows NT
Select the log under Programs -
Select the option Log- Application.
Under Log -
This will overwrite the old events if the log is full.
- General system information
When DigiTool or the Control Builder F is started, the message "Application log file is full" appears.
The message can be acknowledged and work can continue.
- The Windows NT application log is full
All online procedures of a DigiTool session are recorded in the Windows NT application log.
If this log is full, the message appears and no further procedures are recorded.
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment