Measuring precision with DAI04
Problem:Solution
- Allocate adjacent channels
Allocate adjacent active channels and put the inputs that are not allocated together.
- Hardware
If all the channels of a DAI04 are not allocated and the free channels are between connected channels, slight precision errors can occur when the next connected channel is measured.
- Overdriving the A/D transformer
When reading a channel that is not allocated, the A/D transformer reaches a saturation point.When the next connected channel is read, the measurement may be slightly imprecise due to overdriving.
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment