Deletion of display assignments
Problem:Solution
A description of this resolution:
'Deletion of display assignments' resolves the following:
The underlying cause is:
A description of this resolution:
- Delete the display assignments of entered functions.
Before the displays for process operation (standardized IDM display, GCM operator display) and graphic displays in which the display variable 'Controller' has been entered are deleted, the display assignments of the entered functions must be deleted.
'Deletion of display assignments' resolves the following:
- Operator Station
When displays and the display variable “Controller” are deleted, the display assignments are not deleted in the system list. References to displays/display variables that have already been deleted remain in the system.
When the entered loop function is selected for central operation, one of the following error messages is displayed: NO OPERATOR DISPLAY or BAD ENTRY.
The underlying cause is:
- Display assignments are administered centrally by the loop function and not deleted.
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment