Basic initialization of redundant CAR 11 modules
Problem:
"Basic initialization of redundant CAR 11 modules" resolves the following:
Solution
A description of this resolution:
- The system must be disconnected before beginning basic initialization, which deletes all programs from the card anyway.
"Basic initialization of redundant CAR 11 modules" resolves the following:
- Automation
For all redundant units, basic initialization starts with the active unit.
In the case of the CAR 11, this leads to the behavior that the pointer instruments oscillate back and forth, lamps go on and off and the output signals behave in an uncontrolled manner.
The problem occurs only when the CAR 11 modules are used redundantly.
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment