Graphic Editor - Bit selection for binary acquisition modules
Problem:Solution
- Lead a Boolean variable to an OR module.
For this special application, a Boolean variable must be noted at the output of the binary acquisition module and carried on an OR module.
The output of the OR module can then be provided with a bit selection as a Packed Boolean.
- Service Station
Bit selection at the output of binary acquisition modules does not describe the configured bit. Symptoms:
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment