Replacing a CMX 40 or a PBM 90 module
Problem:Solution
- Linking the previously disturbed unit
The subscriber lists in the new unit must be checked as to whether the previously disturbed unit is entered there. If it is not, the new unit must be linked again from the service station.
Cross-Reference:
Service Information 43/65-2340CA: Replacing a CMX
Service Information 43/65-6390AA: Replacing a PBM
- Busnetwork
The subscriber list ist uncomplete after replacing a CMX 40 or PBM module.
The CMX 40 which was disturbed appears not to be linked.
- Some disturbed subscribers does not recognize
After replacing a CMX 40 or a PBM module with a new or basically initialized unit, it is linked (automatically through system package 2.81, otherwise manually). In the process it may occur that it does not recognized some disturbed subscribers. When this subscriber functions properly again, it may occur that it is not integrated in the master transfer, and thus cannot send any data.
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment