PDG parameter data cannot be read
Problem:Solution
- Use the Hazeltine or PDG interface
Readout of parameter data via the Hazeltine or PDG interface.
- System handling
In the case of PDGs on which display channel 1 is not operated the PDG parameters cannot be read via the online monitor in Unix mode.
This especially applies regularly if two PDGs are operated in compatible mode.
The error occurs in the 8.0F/8.0G software and has been eliminated in 8.0H.
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment