The S800 I/O Analog outputs does not provides a bad data quality diagnostic
Problem:Solution
- S800 I/O Analog output now provides a bad data quality diagnostic.
This is fixed as part of the System Services Fixes for Version 3.3/1 fixes.Click Here for the Instructions. To create the diagnostic, the Action On Error attribute must be configured in the AOT FCM to something other than the default of Nothing.
- S800 Analog Outputs do not have Bad Data Quality functionality
It was impossible to detect a bad data quality for the S800 Analog Outputs
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment