The Timer Ladder Logic faceplate failed in beta testing
Problem:Solution
- This is fixed
With MOD300 Connect 2.1 (Part of Operate IT Process Portal B1.0 for MOD300 Connect), the Timer Ladder Logic faceplate was coded with the element type TMR, which worked in development and test but not in the beta test. The faceplate was coded with the correct TIM element type.
- The Timer Ladder Logic faceplate failed in beta testing
- The Timer Ladder Logic faceplate failed in beta testing
The Timer Ladder Logic faceplate was coded with the element type TMR, which did not work in the beta test.
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment