Need a listing of all of the tags in the system.
Problem:Solution
- Generate a listing of all of the tags in the system.
For History configuration reasons, it is sometimes necessary (or nice) to be able to generate a listing of all of the tags in the system.
The function lmtest can be utilized to generate that list. lmtest itself sends output to either std out or errout. Whichever, the output needs to be directed to a file.
at this point, you're prompted to hit return when the system is initialized
- How do I see available tags?
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment