US Robotics Modem Settings
Solution
A description of this resolution:
- How to set Advant-compatible parameters in a US Robotics modem
To display the modem settings for a U.S. Robotics modem, enter the following:
The modem settings that will work with an Advant Station are:
U.S. Robotics Sportster 33600 Settings...
B0 E1 F1 M1 Q0 V1 X1 Y0
BAUD=9600 PARITY=N WORDLEN=8
DIAL=TONE ON HOOK
&A3 &B0 &C1 &D2 &G0 &H0 &I0 &K1
&M4 &N6 &P0 &R1 &S0 &T5 &U0 &Y1
S00=001 S01=000 S02=043 S03=013 S04=010 S05=008 S06=002
S07=060 S08=002 S09=006 S10=014 S11=070 S12=050 S13=000
S15=000 S16=000 S18=000 S19=000 S21=010 S22=017 S23=019
S25=005 S27=000 S28=008 S29=020 S30=000 S31=128 S32=002
S33=000 S34=000 S35=000 S36=014 S38=000 S39=000 S41=000
S42=000
LAST DIALED #:
Switch Settings on the back of the modem should be
S1 - DOWN/ON - Normal DTR Operations
S2 - UP/OFF - Verbose Results
S3 - DOWN/ON - Enables Result Codes
S4 - UP/OFF - Displays Keyboard Commands
S5 - UP/OFF - Autoanswer Enabled
S6 - UP/OFF - Normal CD Operations
S7 - DOWN/ON - Loads &F0
S8 - DOWN/ON - Enables AT Command Recognition
Use the at commands to change any settings to the above.
'US Robotics Modem Settings' resolves the following:
- I need to configure a modem
- Article imported from the previous version of KnowledgeBank
Add new comment