Text editor in HP-UX 10.20:
Problem:Solution
- Graphical Text Editor -MOD
As an alternative to the 'vi' text editor
Text editor in HP-UX 10.20:
There are other useful programs in the usr/dt/bin directory also ( calculator ). You need the graphical environment variables, so if you log in as root, type su root (NOT su - root). The dash ( - ) in the command line tells unix to use the environment variables of the user you are switching to. The root user uses a text base environment.
Text editor in HP-UX 9.0x:
- I need a text editor
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment