AdvaCommand 1.6/0 - static text on graphics is misaligned
Problem:Solution
- Run update script
The problem occurs with graphics whose origin lay in the Multibus system. If graphics are ported to the Canandaigua level OS, static textwill appear slightly (but noticeably) higher on the graphic. The same problem occurs if the graphics were originally ported to Ontario (wherethey worked) and then ported to Canandaigua.
The fix was released in OS1.6/1, and is actually part of the 'updateTo1.9-0' script which is to be manually run at OS1.6/1 install time.
- Trouble with static text on graphics
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment