Backup log file is missing
- Log file is not required
When executing an Ignite-UX back-up from an Advant OS/ES (client) to an Advant OS (server) three files should appear in the '/home/opt/ignite/images' directory after performing the 'os_make_sys_image' script; 'make_sys_image.log', '
Only the ' If
There are only two of the three files in the '/home/opt/ignite/images' directory required to be copied (or backed-up to DAT cartridge) when saving an Advant Station configuration that was created using the 'os_make_sys_image' script. Reference the 'Advant Station 500 Series with AdvaCommand 1.6/1 / AdvaBuild 2.7/0 User's Guide', 3BUR001307R0001 REV F, section '5.3 Full Station Backup and Recovery for AdvaCommand 1.6/1 with Options' on pages 5-18 and 5-19. Copy (using the 'tar' utility) the '/home/opt/ignite/images/Article imported from the previous version of KnowledgeBank
Add new comment