Using osColorChange to modify display
Problem:Solution
- Use color changing procedure
There is a program called osColorChange. It uses a file called hardCopyColor.dat. This file has two columns column 1 is the original color column 2 is the substituted color. The color values can be determined from the Display Builder menus.
This is an example of one that works well. This includes conversions of grayscale-to-black for reverse video. Copy and paste this to 'hardCopyColor.dat' then ftp to your Advant node. Don't forget to add ' -rv ' to the hardCopyScript file (i.e. xpr -rv . . .).
- Can't change screen dump colors
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment