NetNodeCfg has changed since last version
Problem:Solution
- Repair NetNodeCfg
EXTALMxx tags were not working at OS 1.7/1
The problem has been found in OS1.7/1. In previous versions, NetNodeConfig was located in two locations. In this version /etc/opt/advant/MODBase/ does not have the bsNetNodeConfig file. This is where the EXTALMxx gets the node address. The bsNetNodeConfig in /etc/opt/advant/UXBase/ is different.
- AdvaCommand 1.7/1 EXTALMxx tags do not work
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment