Requirements for printing TLL segments and TCL source code
Problem:Solution
- Printing TLL segments or TCL source code to file in ASCII format
Once an ASCII file has been defined in the 'LOG_DETL' and 'PORTS' templates it can continue to be selected as a print device in TLL (using the 'next choice' key), it can be typed into the TCL printer field and successfully printed to file.
- Cannot print TLL segments to a file Cannot print TCL source code to a file
- Article imported from the previous version of KnowledgeBank
Answers
Cause: Article was imported from the previous version of KnowledgeBank Resolution:
Add new comment