MS Excel Error ABB Function
Problem:
MS Excel is not functioning properly after the install. When attempting to open the application, one gets pop up window with compile error in hidden module ABB functions.
Symptoms:- MS Excel not functioning properlyWhen opening excel pop up window with compile error in hidden module ABB functions;
Answers
Cause: The version of MS Excel installed is 2010 64 bit. According to release notes 3BSE067787, MS Excel 2010 32 bit is required for compatibility reasons. Resolution:
The resolution is to uninstall MS Excel 2010 64 bit and reinstall MS Excel 32 bit.
Add new comment