Aspect List
800xA Simulator is loaded but not installed on this node. How can one successfully un-load the extension and remove 800xA Simulator from this list without compromising the integrity of the system.
- Unable to delete simulator from aspect listSimulator was uninstalled from system along with all it's dependencies. However, it was still showing in aspect list
Answers
The simulator software was installed to capture the IO list for the 3rd party Model companies. Also, the AS1 and CS1 were configured with the software to further the configuration of the Simulator.
The simulator is only installed on the OTS system and now the intent is to remove all of the ABB Simulator product off the OTS system.
If the simulator and all of it's dependencies are removed from the system and it's confirmed the system is not compromised, the following procedure can be followed to remove item from aspect list.
Delete dependencies from the Service Structure, Control Structure and Library Structure
Right Click on item - Delete - Say No
The Item will be removed from the list
Please note ( If any dependencies are remaining on the system they will not work). If one is not sure, I will advise not to run this procedure because nothing is compromised with the simulator in the aspect list.
Add new comment