Windows File Indexing
Problem:
Warning
Windows File Indexing (Windows Search) is enabled for the directories (or subdirectories to the directoried) Listed below. It is HIGHLY recommended to turn off Windows File Indexing completely or exclude the directories listed below. This can lead to severe problems during download to the controllers.
C:\ABB Insustrial IT Data
- Windows pop-up error warningWindows File Index pop-up warning
Answers
Cause: Windows File Indexing was enabled Resolution:
On Windows 7 OS, Control Panel, Indexing Options, Modify, C:\ABB Insustrial IT Data, Uncheck box, Click OK,
Add new comment