Cisco Switch
Problem:
System alarms are reporting configured unused port as port down.
Symptoms:
- Unable to remove port down alarmsAn existing configuration on a switch is currently causing port down alarms
Answers
Cause: After a switch configuration, alarms and down port errors are displayed. Resolution:
In Engineering workplace on IT Server Network, Basic Computer Monitoring, Cisco48-port Switch Alert, IT General Property Aspect, Check the parameter AlarmOnOpenPort check the alarm list to see what port is showing down status.
A filtering of the port may eliminate alarm and port down errors.
Add new comment