Advant UNIX Printer Setup
- Printer SetupUNIX Printer Issue
Answers
Below is the Printer Configuration Procedure with UNIX (Advacommand) Operator Stations:
1> Go to System Display Key -> System Config
2> Click Settings(D6) -> Printer Config (D3)
Printer Config Window Opens
3> From Actions Drop Menu select Option "Add Printer Connected to HP JetDirect........"
SAM hpterm window opens
4> Select option ( 3 ) Add printer to local spooler
Next you have to enter the printer name . This printer will have a corresponding IP address
in the host file. If this printer has not been added to the network then you have to complete
option (2) in the SAM hpterm window first
5> Enter the network printer name or IP Address (q = quit) as27 (or 192.36.66.27)
Next you have select the printer type from a list. Use 'spacebar' to scroll list
6> Please indicate as27's printer type (q=quit)? <Enter the corresponding number from the list>
After this the following list of options will be displayed.
1 Lp destination (queue) name: as27_1
2 Status Log
3 Queue Class
4 Job Monitor
5 Default Queue
6 Additional printer config.............
Select an item for change or '0' to configure (q = quit):
I only configure option 1 and option 6
Option 1 allows you to change the default printer name Default is as27_1 Change to Postscript or Hardcopy etc
Selecting option 6 after changing name gives a new list for configuring
1 Model Script [net-genericpc]3printer]
2 Default Printer Language [AUTO]
3 Banner Page [OFF]
4 Postscript Level [Level 2]
Select an item for change, or q when done ?
I only configure option 4 . Select Level 2 for this. Quit when done. This will take you back to the previous list above.
Now select '0' to configure the queue.
Then exit/quit rest.
Now printer should work for screen/hardcopy prints.
Add new comment