Device Functions menu for Device Management P/H does not show up on Client Nodes
Device Functions menu for Device Management P/H for any installed DTM's does not show up on Client Nodes.
1> Device Management Profibus/Hart software components were found installed on all 800xA nodes including clients.
2> DTM's were installed on all 800xA nodes including clients.
3> Device Functions Menu work on 800xA Server Nodes but do not work on 800xA Client Nodes.
Symptoms:- Device Function missing from Context MenuNo access to Device Function
Answers
1> Remove the Client Node from the Domain and readd back to the system.
2> Reapply system software user settings from Configuration Wizard.
These steps resolved the issue of not showing the Device Functions Menu in the Context Menu. This was the only possible solution to this issue. If above described solution does not help then please contact Supportline for further investigation.
Add new comment