Oracle Instance Wizard fails to create instance with following pop-up "The Oracle Instance Wizard has encountered and error. The Oracle Instance is now in an unstable state..."
The Oracle Instance Wizard fails with the pop-up that reads
"he Oracle Instance Wizard has encountered and error. The Oracle Instance is now in an unstable state. Would you like to drop the instance and start over?"
After Oracle instance creation fails, the following is in hsOraInstanceWizard.log:
Starting wizard in creation mode. --
STEP 1: Copy directories Copying directory "C:\Program Files\ABB Industrial IT\Inform IT\History\Ora92Setup" to "C:\oracle" ... Done! --
STEP 2: Initialize EH Provider Modifying "initehprovider.ora" ... Done! Writing "initehprovider.ora" to "C:\oracle\ora92\hs\admin\initehprovider.ora" ... Done! Setting permissions for "C:\oracle ... Done! --
STEP 3: Create a new Oracle instance Modifying "initADVA.ora" ... Done! Running "oradim -new" .... Done! --
STEP 4: Create the Oracle system database
Gathering Oracle table space configuration ... Done!
Preparing to run "ADVA_02_CreateDB.sql" ... Done!
Running "ADVA_02_CreateDB.sql" .... Failed! System.Runtime.InteropServices.SEHException: External component has thrown an exception. at hsOraInstance_Native.InstanceManager.create(InstanceManager* , ConfigFile* , Boolean , Boolean , Int32 ) at hsOraInstance_Managed.InstanceManager.create(ConfigFile configFile, Boolean createHistoryDB, Boolean resume, UInt32 resumeStep) at hsOraInstance_GUI.CreateInstancePage.createInstance() Registry Value ORA_ADVA_SHUTDOWNTYPE = 'a'
Stopping OracleServiceADVA ... Done!
Running "oradim -delete" .... Done!
Deleting directory "C:\oracle\admin" ... Done!
Deleting directory "C:\oracle\oradata" ... Done!
Deleting directory "F:\oracle" ... Done!
Deleting runtime files from %HS_DATA% ... Done!
Symptoms:- Oracle Instance Wizard fails to create instance IM 800xA services will not go to service state
Add new comment