Fail to register PPAtoXML dll error while upgrading to SV5.1 Feature Pack 5.1.1
Problem:
Error loading Feature Pack 5.1.1 on a client "Failed to register PPA to XML dll error" Error code 1904
- Windows pop-up error during installation of Feature PackError loading Feature Pack 5.1.1 on a client "Failed to register PPA to XML dll error" Error code 1904
Answers
Cause: MS Word and MS Excel is not loaded on the nodes that experience this error Resolution:
Appears that MS Word & Excel containing MS Office components is required for PPAToXml.dll to properly register during the auto installation.
Note: MS Word and Excel is not a requirment when upgrading to SV5.1 Rev A. Problem seen only when upgrading to SV5.1 Feature Pack.
Add new comment