Unable to delete unused CBM DIS Signal objects in Control Structure
Problem:
System 800xA V4.1
When try to delete CBM DIS Signal objects in Control Structure, get following errors: Error [ACP Error]: Aspect not found in the object manager. Transaction Cancelled.
Symptoms:
- [ACP Error]: Aspect not found in the object manager. Transaction Cancelled.Unable to delete unused CBM DIS Signal objects in Control Structure
Answers
Cause: Incorrect CBM Signal Type (CBM_DIS Signals) were created under AO810 Module
Resolution:
Resolution:
1> Ran Structure Consistency Check and received "Failed to Access Child object errors in Functional and Control Structures". Incorrect Child links found on those CBM_DIS objects under AO810 module.
2> Corrected the corrupted objects/aspects by running DOS command Afwsct -eh -c
3> Now objects that do not belong under AO810 modules in control structure can be deleted.
Add new comment