DLL Files failing to register after Upgrading to SV5 SP2
Problem:Upgrading from v5.0 SP1 to v5.0 SP2. The base installation fails with several .DLL Files failing to register.Symptoms:
- The base installation fails with several .DLL Files failing to registerCannot finish the upgrade
Answers
Cause: Documentation is inconsistent Resolution: In the System Version 5.0 SP2 Upgrade Manual 3BSE036342R5021 C Section 2 Page 65, a bullets states: "The installation sequence. Install the software in the order listed in Table 2". which implies CLS is upgraded last since it is last in the table. This is contradicted by the upgrade procedure "to update the node:" States that CLS should be un-installed and upgraded first before any other 800xA software is upgraded.
Add new comment